Additional Uplink parameters are described in PUSCH Common (Basic LTE FDD Uplink), PUCCH Common (Basic LTE FDD Uplink), and Sounding Reference (Basic LTE FDD Uplink).
|
1. Cell Parameters |
|---|
Range: 0 to 503
Default: 0
Enter a value for the cell ID. See 3GPP TS 36.211.
Range: 0 to 65535 (0xFFFF)
Default: 0
Enter a decimal value for the Radio Network Temporary Identifier (RNTI).
Choice: 1.4 MHz (6RB) | 3 MHz (15RB) | 5 MHz (25RB) | 10 MHz (50RB) | 15 MHz (75RB) | 20 MHz (100RB)
Default: 5 MHz (25RB)
Double-click or use the drop-down menu to set the system bandwidth and number of Resource Blocks (RB). When you select a system bandwidth, the software automatically adjusts the value in the cell and the cell.
The resource blocks and some parameters are reconfigured by changing the System Bandwidth parameter, similar to when a is executed.
The value in this cell is set by the software based on the setting.
The value in this cell is set by the software based on the setting.
Default: 15 kHz
Displays the subcarrier spacing for the uplink. Only the 15 kHz subcarrier spacing is available in this release.
Choice: Normal | Extended
Default: Normal
Double-click or use the drop-down menu to select a or cyclic prefix. The software sets the based on the cyclic prefix selection.
Default: 12
Displays the number of consecutive subcarriers in the uplink resource block.
Default: 7 for Cyclic Prefix; 6 for Cyclic Prefix
Displays the number of consecutive symbols in the uplink resource block. The software sets the based on the selection.
Choice: Off | On
Default: On
Double-click or use the drop-down menu to turn PUSCH DFT Swap on or off.
PUSCH DFT Swap influences how data is mapped to resource elements in the physical uplink shared channel after discrete Fourier transform is performed. PUSCH DFT Swap can be turned on or off to provide two different interpretations of how data should be mapped to resource elements in PUSCH channels. For details about this feature, contact your Keysight representative.
Choice: Off | Group Hopping | Sequence Hopping
Default: Off
Set one or both of the following parameters to to allow manual control of :
Double-click or use the drop-down menu to select or or to turn hopping .
See 3GPP TS36.211 for more information about Group Hopping and Sequence Hopping.